DRV.NVCHECK

Description

DRV.NVCHECK returns a checksum of all the drives NV parameters. This parameter can be used to detect changes in parameters.

In some applications a controller may need to confirm the AKD2G drive contains an expected set of drive parameters. Reading and checking all the drive parameters individually is viable but this would be a long process involving many reads over the network. DRV.NVCHECK is a checksum on all the NV parameters and this parameter can be read in a single transaction. DRV.NVCHECK will return the same number if all the drive parameters match. If any of the drive parameters are changed then DRV.NVCHECK will return a different value.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

None
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
DRV.NVCHECK

3000h

03h

Unsigned32

-

-

Read only

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

DRV.NVCHECK

2009

7D9

Unsigned32

Read Only

-

PROFINET

Parameter

PNU

Data Type

Access

Units

DRV.NVCHECK

2009

Unsigned32

Read Only

-